IP.MODE

Description

This parameter is used to determine how the drive acquires an IP address for service port communication.

IP Mode Mode of Acquiring IP Address
1 Fixed IP Address: A static IP address is defined by the value set using IP.ADDRESS.
2
(default)
DHCP/Auto IP: Acquires a dynamic IP address using DHCP or Auto IP. If a DHCP server is not available, the drive uses Auto IP to acquire an available IP address.

Recovering communications with a drive on an unreachable IP address

AKD2G drives can be recovered using the display's TCP/IP option. Instructions on how to configure TCP/IP on the drive using the display can be found in AKD2G TCP/IP Configuration.

Examples

Code

Set drive to use static IP of 192.168.0.1

--> IP.MODE 1
--> IP.ADDRESS 192.168.0.1
--> IP.SUBNET 255.255.255.0
--> IP.RESET

Context

For more information on IP configuration, see Finding and Connecting to a Device.

Versions

Action Version Notes
Implemented 02-00-00-000

 

General Information

Type Read/Write
Units N/A
Range 1 to 2
Default Value 2
Data Type Integer
See Also IP.ADDRESS, IP.SUBNET, IP.GATEWAY, IP.RESET

Stored in Non-Volatile Memory

Yes

Variants Supported

All variants supported.

Fieldbus Information

EtherCAT CoE and CANopen

Command

Index

SubIndex

Data Type

Units

Float Scale

Access

PDO Mappable

IP.MODE

3013h

04h

Unsigned16

-

-

Read/Write

No

EtherNet/IP

Name

ID

Hex

Data Type

Access

Units

IP.MODE

2201

899

Unsigned16

Read/Write

-

PROFINET

Parameter

PNU

Data Type

Access

Units

IP.MODE

2201

Unsigned16

Read/Write

-